Trace Chart
Trace data captured from the oscilloscope can be displayed as a Multiple Traces Chart (view multiple waveform traces or measurements) or a Single Trace Chart (view and analyze a single waveform trace or measurement).
Multiple Traces Chart 
                                        The Multiple Traces Chart view displays the selected waveform traces or measurements over time.
                                             
                                        
Single Trace Chart 
                                        The Single Trace Chart view enables you to view and analyze the waveform trace or measurement selected from the drop-down list next to the Single Trace Chart icon. In the Single Trace Chart view only, you can also use vertical and horizontal markers to gather additional information from the selected trace or measurement.